This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ESD122: SOT-723 / SOT-923

Part Number: ESD122

HI Sir 

May I know SOT-723/SOT-923 package can use ESD122 to replace ? (pin 2 pin)

Thanks

  • Hi,

    The ESD122 is not pin to pin with the SOT-723 or SOT-923 packages. The DMX package is smaller than the SOT-723 and the DMY package is in between the SOT-723 and SOT-923.

    Thanks

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.