Data sheet I think that "D1 +, D1-, D2 +, D2-" are connected to correspond N.C in the connection example in the lower figure of Figure 16.
(Example: "D1 +" of 1 pin is connected to "N.C" of 8 pin)
Question:
Although N.C is "not normally connected" and described in the datasheet,
is it possible to connect with other signal lines as shown in Figure 16?
Best regards,
Masumi Sekiguchi