Hi everyone.
I have an issue about voltage and Polarity of USB+Solar power connector on USB Solar Charge project.
In my application, I use 5 pin connector for USB and Solar Power input. But in some case, have an occur when user connect wrong on those pin, such as: put power of solar charge to USB_DP/DN, or inverser btw GND and solar power,... so make circuit burn in those case.
I have just update the overvolatge for solar power small than 28V.
But in this case, if connect power to USB_DP/DN, maybe TVS diode can not protect when not have right VBUS.
Please help me to solve this issue.
Thanks