Hello,
My customer has question below;
TPD5S116 VIL requirement is -0.5V ~ 0.082*Vcca.(0.246V @vcc=3v)
That means output voltage of RK3399 should be under 0.246V to input signal low for TPD5S116.
So strictly speaking, there is possibility for TPD5S116 to judge it high level if output voltage of RK3399 is over 0.246V.
Otherwise, RK3399 VOL spec. is ~0.375V.
That means there is possibility to be up to 0.375V for output voltage of RK3399.
Are there any other means to help solving problems?