Hi,
I'm in midst of looking for a surge protection device for pre-power stage on my audio amp which carries a 9V abs max Vin. My audio amp is currently drawing power directly from battery pack but spikes was detected whenever physical connection of my battery was compromised. I noticed that TVS0500 was capable of f-clamp @ 9.5V, but will it work if i were to clamp forward voltage below 9V? As i noticed TVS family of product tends to operate on much higher Vclamp range, thus i will need some recommendation if TVS0500 may not be applicable in my case here. Thanks.
Regards,
Leo