TPD4E02B04: Is this ESD Protection Diode for USB Type-C pass any level of IEC 61000-4-6 international standard ?

Part Number: TPD4E02B04

Hi! I have a few questions about TPD4E02B04 ESD Protection Diode for USB Type-C,

1.Is this ESD Protection Diode pass any level of IEC 61000-4-6 international standard ?

2.Can you briefly explain is it important for  USB Type-C protection device to pass this standard(IEC 61000-4-6) ?

3.If it's important  , is there any recommend  ESD protection devices for USB Type-C which included this protection(IEC 61000-4-6) ?

Thanks you very much!

 

1 Reply