This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD4EUSB30: Can it use USB2.0 circuit protection?

Part Number: TPD4EUSB30

Hello,

I have two questions about TPD4EUSB30.Please help to solve,

1.Can it use USB2.0 circuit protection?

2.D2+(pin4) and D2-(pin5) swap,it‘s  mean D2+(PIN4) link USB TX0-, D2-(PIN5) link USBTX0+, is it OK?

Thanks.