I am using the code:
psLineCoding->ulRate = 115200;
psLineCoding->ucDatabits = 8;
psLineCoding->ucParity = USB_CDC_PARITY_NONE;
psLineCoding->ucStop = USB_CDC_STOP_BITS_1;
USBBufferInit((tUSBBuffer *)&g_sTxBuffer);
USBBufferInit((tUSBBuffer *)&g_sRxBuffer);
USBDCDCInit(0, (tUSBDCDCDevice *)&g_sCDCDevice);
And when I want to transmit something I send the command:
USBBufferWrite((tUSBBuffer *)&g_sTxBuffer, "OK", 2);
The computer shows me a virtual com port number 37, but when I transmit then computer doesn't receive the characters. What is wrong?
Thanks in advance,
Galbas.
Galbas,
What TI device are you using here?
Regards, Dan
Closing due to no response.