This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Linux/SN65DSI84: Linux driver

Part Number: SN65DSI84

Tool/software: Linux

Hi ,

 do we have any driver for LINUX kernel?

Thanks

Umberto

  • Hello Umberto,

    We are reviewing your question. I will be back with our answer shortly.

    Regards
  • In reply to Joel Jimenez0:

    Hello Umberto
    Contact me to email to provide you a sample code that we use in Linux for OMAP to configure the DSI8x, this code executes the initialization sequence for the SN65DSI8x and configure the device registers.This is only a sample code; the customer needs to modify the values in the code to match the required resolution, video format, etc.
    This sample code can be used to configure the DSi8x devices from Linux and you also can explain to the customer that the DSI interface is fully supported on the OMAP mainline Linux kernel in the following address:
    git.kernel.org/.../dsi.c
    Regards,
    Joel

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.