• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Interface » Consumer & Computing » Consumer & Computing Forum » TUSB1211 - SOF and Clock Output
Share
Consumer & Computing
  • Forum
  • Files
Options
  • Subscribe via RSS
Check out
Analog Wire blog
  • $core_v2_blog.Current.Name

    Cable equalization 101 – Automating your design

    Posted 1 day ago
    by Hooman Hashemi
    Judging by the number of views on a post related to numerical...
  • $core_v2_blog.Current.Name

    RS-485 - Who says you can't teach an old dog new tricks?

    Posted 5 days ago
    by Neel Seshan
    Would you agree that RS-485 has turned out to be one of the most...
  • $core_v2_blog.Current.Name

    Filter for thought

    Posted 6 days ago
    by Soufiane Bendaoud
    Have you ever wondered how engineers designed active filters...

TUSB1211 - SOF and Clock Output

TUSB1211 - SOF and Clock Output

This question is answered
Fred Arnold
Posted by Fred Arnold
on Sep 14 2011 20:08 PM
Prodigy20 points

Hi,

I am interested in the TUSB1211 because of its SOF output pin, which would allow me to synchronize several devices to Start Of Frame.

However, the documentation in the datasheet is poor and there is no reference on how to enable this pin. The only thing mentioned is that it needs to be enabled by setting a flag in a specific vendor register but there is no reference made to any register addresses.

Now to my questions:

1. Is there a register description of the TUSB1211 available which would allow me to utilize the SOF output?

2. Is there any timing information of the SOF output, e.g. jitter and delay between USB SOF and the signal appearing on the SOF pin F6 available?

3. What will the SOF pin do in case the TUSB1211 misses one or several Start Of Frames because of transmission errors?

4. If the TUSB1211 is configured to output a 60 MHz ULPI Clock signal on pin A4, is this clock in phase (locked) to the recovered 240 MHz HS-USB clock?

5. What would be the expected jitter on the 60 MHz ULPI clock output?

 

Any help would be very much appreciated!

 

Regards,

Fred

 

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Fred Arnold
    Posted by Fred Arnold
    on Sep 19 2011 20:18 PM
    Prodigy20 points

    Is there really nobody out there who can answer my questions?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Peter Considine
    Posted by Peter Considine
    on Sep 20 2011 13:03 PM
    Intellectual1755 points

    Hi Fred,

    I was just made aware of your post 30mins ago.

    I am the design lead for TUSB1210 and TUSB1211 products.

    Yes this feature is admittedly poorly documented in the datasheet.

    Please find the following information which should help you with your application:

     

    HS USB SOF (Start-Of-Frame) output clock.

    • SOF feature can be enabled by SOF_EN bit
    • SOF_EN is bit5 of VENDOR_SPECIFIC6 register (address offset 0x8E), default logic low (disabled)
    • Only HS SOF is supported, FS/LS SOF is not supported
    • HS USB SOF packet rate is 8 kHz.
    • SOF pin logic is CMOS-type on VDDIO (1.8V) supply
    • SOF’s generated only when PHY is in receive mode mode
    • SOF’s are disabled until a 1st SOF PID has been detected
    • 480MHz PHY clock is generated by internal PLL based on CLK (60MHz) in “input clock mode”, or REFCLK (19.2MHz / 26MHz) in “output clock mode”
      Missing SOFs are inserted if the next SOF pulse is not received after 7503 cycles of 60MHz clock from PHY (which is 480MHz PHY clock divided-by-8)
      • This is to ensure that a "missing SOF" is only ever inserted after 125us is guaranteed to have elapsed based on fastest possible clock 60MHz+500ppm.
      • Note that if a missing SOF is inserted then SOF detection is ignored for the next five 60MHz clock cycles to ensure a double SOF is never generated    
    • Rising edge of SOF output clock signal is synchronized on 60MHz. This is the edge to be used by systems making use of TUSB1211 SOF pin.
    • Falling edge of SOF output clock is synchronized on internal CK32K such that minimum SOF “high” duration is 1 period of CK32K
    • SOF jitter corresponds to 60MHz and 480MHz jitter of 208.33ps max (see chapters 7.1.2.2 and 7.1.15.2 of USB2.0 specification) 
    • Delay from SOF packet to SOF pin rising edge is a fixed deterministic delay but I do not have this number today. We would need to check in simulation. 

    Currently TUSB1211  full datasheet can be distributed only under NDA (Non Disclosure Agreement). I need to check if your company has one in place with TI? Could you please contact your local TI representative. Failing this please send an email to me at p-considine@ti.com and we can discuss your requirements further.

    Looking at your specific Q's:

    1. Is there a register description of the TUSB1211 available which would allow me to utilize the SOF output?

    [Peter] Please see above.

    SOF_EN is bit5 of VENDOR_SPECIFIC6 register (address offset 0x8E), default logic low (disabled)

    2. Is there any timing information of the SOF output, e.g. jitter and delay between USB SOF and the signal appearing on the SOF pin F6 available?

    [Peter] Please see above

    3. What will the SOF pin do in case the TUSB1211 misses one or several Start Of Frames because of transmission errors?

    [Peter] Please see above

    4. If the TUSB1211 is configured to output a 60 MHz ULPI Clock signal on pin A4, is this clock in phase (locked) to the recovered 240 MHz HS-USB clock?

    [Peter] Please see above. The SOF signal is synchronized with 60MHz clock. 60MHz clock is derived from internal 480MHz clock. The internal 480MHz PHY clock is not recovered from USB data. It is generated independently by the PHY but its phase is set in order to optimise data recovery, and its drift meets USB2.0 requirements (as described in HS eye diagram description of USB2.0 spec chapters 7.1.2.2 and 7.1.15.2 ) .  

    5. What would be the expected jitter on the 60 MHz ULPI clock output?

    [Peter] Please see above.

    I hope I have answered most of your questions. Please contact me if you need further information.

    Best regards,

    Peter

    SOF
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • 1962332
    Posted by 1962332
    on May 01 2012 07:58 AM
    Prodigy150 points

    Is there a good reference schematic for using this part in host only mode?   I'm assuming the default configuration (base on datasheet) is host mode.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • 1962332
    Posted by 1962332
    on May 02 2012 07:41 AM
    Prodigy150 points

    Some background.....  We switched from this part SMSC USB3322 (Used on original beagleboards) to the TUSB1211.  Are there any key design differences that we should be aware of making that work with a OMAP.  We originally assumed it was a drop in, but it doesn't seem to be working (can't access registers over ULPI interface and no negotiation for devices that are plugged in).

    I just noticed, that from the spec both CS pins maybe should be pulled up.  If you read about CS_N first, you would tie it to ground, but looking at CS, it notes that CS_N might be pulled high (or maybe low) when CS is high for normal operation. 



    .

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Fabian Stel
    Posted by Fabian Stel
    on May 15 2012 07:35 AM
    Intellectual2090 points

    => Regarding CS and CS_N please find bellow the way to use it:
    - CS : Active-high chip select pin. When low the IC is in power down and ULPI bus is tri-stated. When CS is high (and CS_N pin is Tie to VDDIO if unused.s low) normal operation.
    - CS_N : Active-low chip select pin. When high the IC is in power down and ULPI bus is tri-stated. When CS_N is low (and CS pin is high) normal operation. Tie to GND if unused.

    Please refer to http://www.ti.com/product/tusb1211 document Table 2-1. Terminal Functions.

    => Please find bellow a reference schematic :
    3542.TUSB1211 in ULPI output clock mode.pdf

    => Please find bellow a Basic low-level test to check TUSB1211 device is alive?
    Otherwise if it is very low-level testing you are referring to then you should bias TUSB1211 as in the application diagrams shown in TUSB1211 spec:
    -       Apply VBAT (2.7V ~ 4.8V)
    -       Apply VDDIO (1.8V)
    -       Check CS, RESETB pin levels are VDDIO, CS_N is at GND
    -       Set REFCLK (output CLOCK mode), or CLOCK (input CLOCK mode).

    • If output clock mode check REFCLK is applied correctly, e.g.,  for 26MHz input at REFCLK, REFCLK should be square-wave at VDDIO level, CFG pin tied to VDDIO.
    • If input clock mode check CLOCK is applied correctly, 60MHz square wave at VDDIO level; and CFG pin tied to GND or VDDIO (don’t care which)

    -       Verify DIR goes High->Low (~3ms after CS enabled, which indicates that TUSB1211 PLL has locked, and bus is now in TX mode, i.e., control is given to Link)
    -       Verify 60MHz clock is observed on CLOCK pin
    -       Verify VDD33, VDD15 LDO power supply outputs are in spec (3.1V, 1.5V respectively)
    -       Verify IDDQ vs IDDQ table in TUSB1211 datasheet

    • The objective here is to check that a reasonable current is being drawn from VBAT indicating that internal circuitry (PHY, PLL, biasing, etc) has powered up(if no current or a few 10’s of uA only were drawn this would indicate an issue).
    • When TUSB1211 is powered on, the PHY circuitry will power up in FS synchronous mode albeit without data activity, and IDDQ should exhibit VBAT current draw slightly less than the 31mA given in the datasheet. Typically we measure  about 27mA in the lab.

    -       Verify VBUS is at 5V

    • This is just a check for VBUS presence in the system if this is possible before SW availability.
    • In Device mode : VBUS is expected to be provided at the USB connector by the connected Host. Check (by probing if possible) VBUS arrives at TUSB1211 pin.
    • In Host Mode: VBUS is provided by the Host system. If TUSB1211 PSW pin is used to control  an external VBUS source then VBUS will not be present unless SW has written to the DRVVBUS register bit. If TUSB1211 PSW pin is unused then check if elsewhere in  system VBUS is provided and is present.

    -       Verify DIR goes High->Low
    -       Verify VDD33, VDD18 LDO power supply outputs are in spec
    -       Verify IDDQ vs IDDQ table in TUSB1211 spec

    => IMPORTANT:
    Some informations regardin TUSB1211 are TI-Confidential, not for public distribution.
    Could you please enter in contact with your TI Field Application Engineer in order to put an agrement in place? 

    Best Regards,
    Fabian
    Kindly click the Verify Answer button on this post, if it answers your question.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • 1962332
    Posted by 1962332
    on May 15 2012 15:27 PM
    Prodigy150 points

    We went through and verified each of the steps.  Everything looked good, with the only exception being the DIR which doesn't seem to be low for much time other then a blip after power on and after we toggle reset.  Is there any additional guidance for making this chip work with a OMAP in host mode?  We'd really like to use this chip over the SMSC part used on the BeagleBoard.

    Another question we had was if we could get the power sequencing information (Section 9.3.3.1) mentioned in the datasheet on page 14?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Fabian Stel
    Posted by Fabian Stel
    on May 16 2012 03:17 AM
    Intellectual2090 points

    Again, i am refering to NDA doc regarding TUSB1211. This is TI-Confidential, not for public distribution.
    Could you please enter in contact with your TI Field Application Engineer in order to put an agrement in place? 

    I guess Salmi, Jake is your contact?

    Best Regards,
    Fabian
    Kindly click the Verify Answer button on this post, if it answers your question.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • 1962332
    Posted by 1962332
    on May 16 2012 06:16 AM
    Prodigy150 points

    Yes Jake Salmi is my contact.  He provided me with a application guide and we evaluated that against our design.  I'll send him a copy of our schematic.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • 1962332
    Posted by 1962332
    on May 31 2012 09:21 AM
    Verified Answer
    Verified by BrandonAzbell
    Prodigy150 points

    Thanks for that hardware checkout.  After performing that we found we had one data line getting repinmuxed after the OS booted.  Once that was fixed it worked. 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use