Hello,
Please tell me the input impedence and capacitance at tx_clk and other pins of tusb1310a. I am providing differential clock from controller to the phy using SN65LVDS4 lvds receiver but its output is getting heavily attenuated as the swing becomes 0.5 - 1.2 V in place of 0-1.8V. It seems that it is not able to drive the capacitive load.
Regards,
Ashish
You can find the impedance and capacitance on the ibis model available at http://www.ti.com/product/tusb1310a#technicaldocuments
In this case, for TX_CLK, Rpin = 0.139 ohm and Cpin = 0.738 pF
Regards.