Hello....my Englisg is not good....
My TUSB2036 Device have problem .
I connect it to computer,then after a few seconds it enter suspend mode.
this is my design:
DP0 DM0 (connected to 30 ohm resistor to upstream USB port,and respectively connected 22pf Capacitance to GND.)
NPINT = 00 (no permanently attached devices)
NP3 = 0
EXTMEM = 1 ( No ROM)
DP0PUR (1.5K resistor to DP0)
Xtal1 (connected to 6Mhz resonator)
Xtal2 (connected to 2.2K resistor then connected to 6Mhz crystal)
Mode = 0 (6Mhz)
BUSPWR = 0
OVRCUR 1-3 respectively connected to 15K resistor then connected to 3.3V (doesn't need overcurrent protection)
Reset (connected to 15k and 10uF to create reset signal.)
EEDATA/GANGED = 0
OCPROT/PWRSW = 0
All Downstream Ports +5V are Connected together.