Is the SN65LVDS324, support also 30FPS?
If not, which device can?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello eli,
The SN65LVDS324 has a maximum frame format of 1080p60 (60Hz), and works with a clock from 18.5MHz to 162MHz, so the device is able to handle any video format within the previous clock frequencies.
Regards,
Diego.
Front input SN65LVDS324 is connected to SONY CMOS SENSOR, input 5000000 pixels,30F, can you give me to provide the driver source code?
Thanks a lot.