I'm considering using a TFP401A in an application for an HDMI input (which has no HDCP.) The input may or may not have an audio channel. I don't need this channel decoded, but I do need the video. From one post I read on this forum, it seems audio in the HDMI stream might cause issues, but video alone should work... the post wasn't 100% clear on this though. Would an audio stream prevent proper decoding of the video?
Any information appreciated