Hello
I need to realize a USB HUB with 20 - 40 ports.
Power will be supplied separately.
It will be used for run BITCOIN device like bitfury ecc.
Look here: https://bitcointalk.org/index.php?topic=418087
Can you help me?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I need to realize a USB HUB with 20 - 40 ports.
Power will be supplied separately.
It will be used for run BITCOIN device like bitfury ecc.
Look here: https://bitcointalk.org/index.php?topic=418087
Can you help me?
Thanks
Hello Giuseppe,
The TUSB2077A hub provides up to seven downstream ports in compliance with the USB 2.0 specification as full-speed. Also, the TUSB8040A1 which is a four-port USB 3.0 hub but it is also compatible with USB High-Speed.
You can use a multi-tier configuration ( 6813.Bus_topology.zip).
Regards.