Hello,
I posted this question before and it closed. But I have a another question.
It is mentioned that "The package/case size of these capacitors should be no bigger
than 0402" on the layout guideline.
But my customer uses a 1005 size. It means a 1mm x 0.5mm. (JIS standard)
Does the size 0402 mean 0.4inch x 0.2inch? (EIA standard)
If the recommend size is 0.4inch x 0.2inch, my customer observes the guideline.
Regards,
Naoki Aoyama