We are starting to have difficulties installing the driver 6.7.2.0 on both Windows 7 and 8 systems. Not all systems are having these problems but most are. We have modified the files for our own VID and PID, and we have signed them so we are not having driver signing problems.
The problem is that in some cases the driver installation appears to succeed normally, but when our product is connected to the PC's USB port Windows churns for awhile but then says that the driver was not installed. In other cases, some of the files fail to copy during setup.
The only solution is to go into the Device Manager, select the device, right click and Update Driver. Browsing to the folder that contains the proper files seems to get things to work.
This just started happening a couple of months ago. Is it related to some recent Windows update?
Is this happening to anyone else? Is there a fix?
Thanks for any and all help.
Joe