Hi,
I am struggling with the interface to an TFP403 (part of an FMC-DVI card from Avnet).
When connected to a DVI HD-source, the signals H/Vsync and CLK and DE are coming out, and
look good (1920x1080p50). Also the SCDT is active (because of the active DE).
However all the 24 data pins remain constant : value of the 24-bit word stays 0x010101
(measured at the pins of the TFP403). This does not represent the HD-video input.
Any idea ? What to check ? What to do ?
wkr
Eddy