Hi all,
Would you mind if we ask TUSB2046BVF, TPS2071DAP?
<Question1>
About TUSB2046BVF, we don't use following pins and, we set as followings;
- EECLK(5): be left floating (unconnected)(as the datasheet shows)
- EEDATA/GANGED(6): be left floating (unconnected)
- #EXTMEM(26): High(3.3V)
- SUSPND(32): be left floating (unconnected)
<Question2>
About TPS2071DAP, we don't use following pins and, we set as followings;
- NC(1,4,8): be left floating(the datasheet shows "No internal connection", if these pins are conncted to GND,
will DISSIPATION RATINGS be improved or not?)
- SP(6,7): be left floating (unconnected)
- GATE(10): be left floating (unconnected)
- BP_DIS(31): be left floating (unconnected)
Is our recognition correct? Could you let know us these?
Kind regards,
Hirotaka Matsumoto