Dear Sir:
Could you help to check design SN65LVDS324 + OV5658 can 5M/30fps or others fps?
SN65LVDS324ZQLR parallel to OV5658.
Please kindly help it,
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir:
Could you help to check design SN65LVDS324 + OV5658 can 5M/30fps or others fps?
SN65LVDS324ZQLR parallel to OV5658.
Please kindly help it,
Thanks.
For OV5658 datasheet,I already send to elias.villegas@ti.com.
5M->5megapixel 2592 x 1944,
Please kindlt help to check email,Thanks.
Hello Jason,
We need more information regarding the OV5658, this is because the SN65LVDS324 is specifically made for Sony and Panasonic LVDS formats, so we need to confirm this sensor compatibility. Also I noticed that the maximum MIPI data rates for full resolution are beyond the limits of the SN65LVDS324, Could you confirm if this maximum values are required for the full resolution?
Best regards,
Diego.