Hi,
I have a question about XIO2001.
At my customer's system, they are using XIO2001.
In an evaluation test, the deadlock of OS has occured and
they are searching what cause the deadlock.
They are guessing that the deadlock will occur when XIO20001 is in a high loading state.
Because it occurs when increasing the load of PCI card but
decreasing the load of PCI card, the deadlock won't occur.
XIO2001 supports six PCI bus devices but they are only connecting 3 PCI bus devices
and the PCI bus clock is 33MHz.
Is there any information about the same phenomenon?
If there is a factor which can be considered, please let me know.
best regards,
g.f.