Hello,
i hope You can help me with this.
USB HUB TUSB2077A is configured as :
i connected a pull- up 1.5k resistor on DP0.
- Self-Powered ( /BUSPWR == GND ), no external power
- No EEPROM ( /EXTMEM == VCC )
when i connected downstream device(which is self power) to this HUB, the PC device manager shows the VID&PID of downstream device, but have a question mark on this downstream device.
then power off HUB and set the /BUSPWR == VCC, still no external power (just trick the TUSB2077A), the downstream device is OK to enumerate.
so my question is what is the different when i connect /BUSPWR to VCC or GND. and why this happened?
Jianyang