I have been trying to make TUSB2046 working, but yet no effects.
1st of all I read almost all threads about issues with this chip, modify my scheme even as ppl suggested and still not working.
I am using this chip on bigger scheme, but because it is not responding I am trying to build minimal scheme (minimal.pdf) in which TUSB2046 will be detected by PC.
I pull up all OVRCUR pins and pull down all DP/DM pins (except upstream). The power up sequence meet datasheet requirements (rst.bmp -> yellow power | white Reset | blue XTAL (6MHz if I zoom it). What's wrong still?
I can see that if I power this, after few try's of comunicate PC<->chip TUSB2046 go into suspended mode (pull it HI, and disable XTAL), but If I don't connect RESET to output from comparator it doesn't go into suspended mode and crystal is oscillating as long as I don't pull RESET HI. But no matter what I do I can't communicate with it.
Log when connected to PC:
[19600.068053] usb 7-1: new low-speed USB device number 15 using uhci_hcd
[19600.192048] usb 7-1: device descriptor read/64, error -71
[19600.416036] usb 7-1: device descriptor read/64, error -71
[19600.632045] usb 7-1: new low-speed USB device number 16 using uhci_hcd
[19600.752053] usb 7-1: device descriptor read/64, error -71
[19600.976048] usb 7-1: device descriptor read/64, error -71
[19601.192053] usb 7-1: new low-speed USB device number 17 using uhci_hcd
[19601.600029] usb 7-1: device not accepting address 17, error -71
[19601.712053] usb 7-1: new low-speed USB device number 18 using uhci_hcd
[19602.120028] usb 7-1: device not accepting address 18, error -71
[19602.120075] hub 7-0:1.0: unable to enumerate USB device on port 1
minimal.pdf