Dear team,
I've been told that the MINIMUM peak-to-peak input differential voltage in the datasheet (300mV) is VID after the RX equalizer.
Then, what if VID after the equalizer is less than 300mV?
My customer said the peak-to-peak input differential voltage will be 70mV and data rate is 2.7Gbps (HBR). In the datasheet, the maximum EQ gain at HBR is 9dB.
So VID after the equalizer will be 70mV x 9dB = 70mV x 2.81 = 196.7mV which is less than 300mV. Is my understanding right?
In this situation, is it impossible for DP130 to re-drive the signals?
Actually, I've asked this question many times but haven't received the clear answer.
Your clear answer will be very appreciated. Thanks.
Best regards,