Can the TLK3101 be used for gigabit ethernet?
Thanks,
Mircea
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mircea,
TLK3101 does not support Gigabit Ethernet, this device operates from 2.5 to 3.125Gbps (Backplane application) . This device uses the 8b/10b encoding algorithm that is used by fiber channel and gigabit ethernet, although, this process is transparent to the user as the TLK3101 internally encodes and decodes the data such that the user reads and writes 16bit data.
Otherwise, you could take a look in another devices that support Gigabit Ethernet standard and select the best device according your requirements such as follows:
TLK1211
TLK1221
TLK2201
TLK1201
TNETE2201
TLK2208
TLK2206
Best Regards!
Luis Omar Morán Serna
High Speed Interface
SWAT Team
Hi Mircea,
TLK1501 does not support Gigabit Ethernet, this device is intended for high-speed blackplane applications. Otherwise, you could take a look into TLK1201A or TLK1221, that operates from 0.6 to 1.3Gbps. There are several options of devices that support Gigabit Ethernet standard.
I hope this helps.
Best Regards!
Luis Omar Morán Serna
High Speed Interface
SWAT Team