Hi,
I am planning to use the TLK10034 Evaluation Module (EVM) for providing multiple high-speed serial inputs to a transmitter IC. I see that the high-speed Tx outputs for channels A & B in the evaluation module come out in SFP modules. Is it possible to remove those modules and bring out these outputs to SMA connectors instead? Is it possible to specify this when purchasing the EVM? Otherwise one needs to use SFP to SMA adapter and that might cause difference in the characteristics of channel A &B outputs compared to channels C & D. I am asking because my application requires all four channels to transmit (random) data that are synchronized and have identical frequency characteristics.
Also, can the low-speed inputs to the EVM be interfaced with PCI Express?
Thanks,
Anandaroop