This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
<aardvark>
<configure i2c="1" spi="1" gpio="0" tpower="1" pullups="0"/>
<i2c_bitrate khz="100"/>
======Select Page 0======
<i2c_write addr="0x5E" count="1" radix="16">FF 00</i2c_write>/>
======Select PRBS7 pattern. ======
====== PRBS7: 0x01 ====
====== PRBS11: 0x09 ====
====== PRBS15: 0x21 ====
====== PRBS20: 0x39 ====
====== PRBS23: 0x11 ====
====== PRBS31: 0x19 ====
<i2c_write addr="0x5E" count="1" radix="16">10 01</i2c_write>/>
======Load pattern on lanes 1 thru 3 for SWAP. ======
<i2c_write addr="0x5E" count="1" radix="16">16 E0</i2c_write>/>
====Read BERT CNT[11:0]======
<i2c_write addr="0x5E" count="0" radix="16">18 </i2c_write>/>
<i2c_read addr="0x5E" count="2" radix="16">00</i2c_read>/>
======Clear BERT_CNT. ======
<i2c_write addr="0x5E" count="1" radix="16">15 10</i2c_write>/>
</aardvark>