This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1210 Vbat recommended voltage

Hi,

one of my customers is asking what should be the voltage of Vbat if Vdd33 is shorted to Vbat externally. He is confused because we suggest different voltages on the DS:

1. first we say that Vbat shouldn't be under 3.3V

2. then we say that Vbat min is 3.05V

3. And we also give the following range for Vbat 3.2-3.6V

Which would be the recommended voltage for Vbat, and why are several different voltages recommended?

What would be the recommended voltage for Vbat when Vdd33 is supplied by the internal LDO?

thanks,

Tadeo