Hi Team,
Could you help review TUSB211 schematic review?
Thanks,
Scott
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Could you help review TUSB211 schematic review?
Thanks,
Scott
The TUSB211 is designed as not to break the USB DP and DM traces, pin 1 should connect to pin 8, and pin 2 should connect to pin 7 (Pins shorted by running traces underneath the part). Please refer to section 10 of the datasheet for routing info.
We also recommend to start with a lower EQ setting (EQ1) of 1.7K Ohm. This can be increased to 3.9K if the eye-opening is not sufficient.