Hi Team,
The customer is using TMDS442. Look the attachment, it is the schematic. LC_SCL pin and LC_SDA pin are added a 4.7K pull-up resistor to 3.3V on his PCB board. The schematic is not drawn. When the HDMI video signal is input to TMDS442, the 5V_PWR1(3) pin is 5V and it is normal, but the 5V_SINK1(67) pin is 3.3V,not 5V. I2C_WriteByte is 0x18,0x01,0x5C. 01 is the register model, 5C is the device address and 0X18 is the data.
Q1:Is the 3.3V voltage for the 5V_SINK1 pin normal?
Q2: Is the schematic correct?
Q3: Is IIC configuration correct?
Thanks,
Best Regards,