Hi:
TLK10232 now can working at 10GBASE-R SFP+, but cannot link when configures in 1000BASE-KX mode; Our system configurations and registers status are below:
Board connection: SWITCH-BCM56820(serdes)<-------->TLK10232(1000base-kx)<-------->SFP
RefCLK: 156.25MHZ
MODE_SEL pin = LOW
ST pin = LOW
PRBSEN = LOW
Configurations:
mdio write 0x1e 0x0000 0x8610
mdio write 0x1e 0x0000 0x0e10
mdio write 0x1e 0x001D 0x2000
mdio write 0x07 0x0000 0x0000
mdio write 0x01 0x0096 0x0000
mdio write 0x1e 0x0001 0x0300
mdio write 0x1e 0x0002 0x831B
mdio write 0x1e 0x0003 0xAA4E
mdio write 0x1e 0x8020 0x03ff
mdio write 0x1e 0x8021 0x010F
mdio write 0x1e 0x0004 0xD560
mdio write 0x1e 0x0006 0x1114
mdio write 0x1e 0x0007 0xDD05
mdio write 0x1e 0x000e 0x0008
Register dump:
------------------------(Dev 0x1)------------------------
[0000] 0x0000 [0001] 0x0002 [0002] 0x4000 [0003] 0x5100 [0004] 0x0011 [0005] 0x000B [0006] 0x4000 [0008] 0xB000
[000A] 0x0001 [000B] 0x0050 [0096] 0x0000 [0097] 0x0000 [0098] 0x0000 [0099] 0x0000 [009A] 0x0000 [009B] 0x0000
[00A1] 0x3001 [00AA] 0x0003 [00AB] 0x0000 [00AC] 0x0000 [00AD] 0x0000 [00AE] 0x0000 [00AF] 0x0000 [8001] 0xCC4C
[8002] 0x0000 [8003] 0x0000 [8005] 0xCE00 [8006] 0x0000 [8007] 0x0000 [8008] 0x0080 [8010] 0xFFFD [8011] 0xFFFD
[8012] 0xFFFD [8013] 0xFFFD [8014] 0xFFFD [8015] 0xFFFD [8016] 0xFFFD [8017] 0xFFFD [8018] 0x0000 [8019] 0xFFFF
[801A] 0xFFFF [801B] 0xFFFF [801C] 0xFFFF [801D] 0xFFFF [801E] 0xFFFF [9001] 0x0200
------------------------(Dev 0x3)------------------------
[0000] 0x0000 [0001] 0x0002
[0008] 0x8001 [0020] 0x0004 [0020] 0x0004 [0021] 0x0000 [0022] 0x0000 [0023] 0x0000 [0024] 0x0000 [0025] 0x0000
[0026] 0x0000 [0027] 0x0000 [0028] 0x0000 [0029] 0x0000 [002A] 0x0000 [002B] 0x0000 [8000] 0x00B0 [8010] 0x00FD
------------------------(Dev 0x7)------------------------
[0000] 0x0000 [0001] 0x0088 [0005] 0x0080 [0010] 0x1001 [0011] 0x0080 [0012] 0x4000 [0013] 0x0001 [0014] 0x0000
[0015] 0x0000 [0016] 0x2000 [0017] 0x0000 [0018] 0x0000 [0019] 0x0000 [001A] 0x0000 [001B] 0x0000 [0030] 0x0003
------------------------(Dev 0x1e)------------------------
[0000] 0x0E10 [0001] 0x03BC [0002] 0x831B [0003] 0xAA4E [0004] 0xD560 [0005] 0x2000 [0006] 0x1114 [0007] 0xDD05
[0008] 0x000D [0009] 0x0380 [000A] 0x4000 [000B] 0x0D10 [000C] 0x0371 [000D] 0x2F80 [000E] 0x0000 [000F] 0x1453
[0010] 0x0000 [0011] 0x0000 [0012] 0xFFFD [0013] 0xFFFD [0014] 0xFFFD [0015] 0x8180 [0016] 0xF083 [0017] 0x2000
[0018] 0x0C20 [0019] 0x2500 [001A] 0x4C20 [001B] 0x1020 [001C] 0x0000 [001D] 0x2000 [001E] 0x0000 [001F] 0x0000
[8003] 0x0283 [8004] 0x017C [8020] 0xF3FF [8021] 0x010F [802A] 0x02FD [802B] 0x02FD [802C] 0x0207 [802D] 0x02FD
[802E] 0x02FD [802F] 0x0207 [8040] 0x0000 [8041] 0x0000 [8042] 0x0000 [8100] 0x0000 [8101] 0x0000
Is there any suggestion?