Other Parts Discussed in Thread: TLK3134
Dear support team,
Our customer is evaluating TLK1211 now.
I got the following questions from the customer.
So please give me some advice.
Questions:
1. In the table in page 12 of the datasheet, the following values are indicated in the parameter which is
V(CM) Receiver input voltage requirement, VID = | RxP - RxN |.
Min: 200mV
Max: 1600 mV
Is the above value not peak to peak but single phase amplitude?
Is this understanding correct?
2. Could you teach the value that is output as JTAG ID code when boundary scan test is performed
by connecting TLK1211 RCP to the JTAG chain?
Best regards,
M. Tachibana