Other Parts Discussed in Thread: TLK10232
Hello,
we want to design system with data rate 10Gbps(max distance 20km), the transceiver chip will be connected to FPGA and SFP+ optical module. can TLK10031 be used for the application?
Thank you,
Kerb
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kerb,
The TLK10031 is able to interface with optical modules through 10GBASE-SR or 10GBASE-LR. The distance that you are planning to use is too long for these physical layers. Please let me verify with the team if this is feasible with this device.
Best Regards,
Luis Omar Moran
High Speed Interface
SWAT Team
Hello,
Optical interface of The SFP+ Optical Transceiver is compliant to IEEE 802.3ae 10GBASE-LR, is it ok?
Thank you,
Kerb