Hi:sir,
we were using the SN65DP159 chip to adjust the video signal out from windows xp GPU,the bandwidth is 5.4Gbps(image resolution 3840x2160,60Hz),but the image we got from SN65DP159 to display is blinking,seems like the signal from SN65dp159 is not very well,we try to fix it by edit some register like Reg0CH and REG0x4D,but the image still not very stable,so how to adjust the SN65DP159 register to the promote the signal quality to make the image stable?