Hi Team,
Please allow me to clarify the settings and the operation of TX termination control using TMDS181.
Q1). Does the device automatically choose the TX termination resistor as shown in the TX_TERM_CTL pin settings, when setting the pins in the following condition ?
- Pin10: I2C_EN/PIN = High (I2C Enable)
- Pin26: TX_TERM_CTL = NC (Floating is Automatic Select Mode)
Customer does not see the device operating in "automatic select mode" using the EVM.
Q2). Customer set the TX_TERM_CTL register through EyeScan Tool, however, TX termination resistor did not change. Is there any override bit for this register setting to work prior to the pin setting ?
Please also advise us which asked in the following post.
https://e2e.ti.com/support/interface/digital_interface/f/130/t/588766
Since customer is in a hurry, it would be helpful if you could give us your comments by 4/17 (PST).
Thanks in advance.
Best Regards,
Kawai