Hi TI,
I detected a 4K signal problem,
Under default condition of TMDS181EVM,
Pin |
Items |
set |
1 |
HDP_SRC |
JP 1-2 for not used |
J3 |
I2_EN_PIN |
JP 2-3 for pin strap |
J4 |
SCL |
JP 1-2 for USB IF TO I2C |
J6 |
SDA |
JP 1-2 for USB IF TO I2C |
J7 |
A1 |
NC for weak internal pulldown (Normal Mode) |
J8 |
VSADJ |
JP 1-2 for 6.8KΩ |
J11 |
SIG_EN |
JP 2-3 for Signal Detect Enable |
J12 |
EQ_SEL_A0 |
NC for Adaptive EQ |
J14 |
TX_TERM_CLT |
NC for auto select of term |
J15 |
PRE_SEL |
NC for 0 dB |
J17 |
SWAP_POL |
NC for normal |
Input 4K signal(Non HDCP) to the EVM, Undre Hot plug condition of the input HDMI cable.
Some time The output was NG(May be Lower rate signal is detected) as lower picture.
This is OK signal(4K)
This is NG output signal( When a Display receive the signal, it cannot draw a picture.)
Do you estimate the origin of the problem ?