Hi team,
My customer is going to use TMDS181 as signal source distributor etc.
And the customer wants to use TMDS181 Eye Scan function.
So, the customer evaluated TMDS181RGZEVM Eye Scan fuction with Eye Scan tool.
The customer got eye diagram when DDC was input to TMDS181RGZEVM,
but couldn't get it when DDC wasn't input to TMDS181RGZEVM.
The customer has following two questions.
(1) Can we get eye diagram from TMDS181 when DDC isn't input to TMDS181?
(2) If we can get it from TMDS181 without DDC, is it due to Eye Scan tool
that it can not be done with TMDS181RGZEVM without DDC?
Please let me know the answers.
Best regards,
Fumio Nakano