This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SN75DP159: SNx5DP159/149 HDMI output specifications

Part Number: SN75DP159

For SNx5DP159 , SNx5DP149 what is the  HDMI out/pair data rate and HDMI Pixel rate

  • Hi Bhavesh,

    DP159 is intended for HDMI2.0, it supports data rates up to 6Gbps, this is enough for 4k@60Hz 24bpp.
    DP149 is intended for HDMI1.4, it supports data rates up to 3.4Gbps, this is enough for 4k@30Hz 24bpp.

    Regards

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.