Hi,
We have implemented the TMDS181 4K HDMI Retimer to our design and have some concerns after noticing that the retimer would fail. We see that the retimer is working fine at first, however, it would eventually stop working . We have been switching different camera inputs into the retimer and are wondering if doing so is causing damage to the retimer regarding the DDC lines. Here's how we have the retimer DDC pins set up on our design (note, we are using pin strap and is close to the configuration as Figure 36):
1.) DDC_I2C _SRC connected to GND
2.) DDC_I2C_SNK connected to the cameras DDC_I2C lines and going to our receiver application
Here are the type of cameras we are using:
1.) Regular HDMI camera
2.) Custom HDMI Camera
We are using the retimer as a sink side application. However, on our custom HDMI Camera, we decided to use the DDC_I2C lines as a way to communicate to the camera to obtain information. We are afraid that switching from a regular COTs camera to our custom camera might be damaging the DDC_I2C lines in the retimer and causing issues within the chip, thus leading to the chip to fail overall. Do you think that might be an issue? Also, could we, in theory, not have anything connected to the DDC_I2C_SRC/SNK pins of the retimer? Would it be possible to just bypass them?
Thanks