Other Parts Discussed in Thread: DS90C383
We have built a customer HDMI board based on the TFP401 IC with LVDS out using the DS90C383 LVDS transmitter. We are connecting to a standard Windows 10 laptop for an HDMI source. On 6 bit (3 stream) LCD the color are displayed correctly. We have a customer that tried to use our board on the attached 8 bit (4 stream) LCD reading the EDID directly from the panel and the colors are off. We have reviewed the color mapping from the 401 to the 383 and they are following the correct MSB pattern. We are stumped as to why the 4th stream is causing the color issues in the photos.
Note: if we disconnect the 4th link (essentially 6 bit data) the colors are fine but the panel is 25% of normal brightness.
8 bit image then 6 bit (dark image)