Other Parts Discussed in Thread: TFP401
Hello,
I am bit new in HDMI/24bit RGB display Interface. My project requirement is as following.
Step 1. Use MSP4032 controller as front end ADC(24 channel with 1 msec sample rate ) and transfer the data via SPI to one of Linux based board . ( beagle bone black/ raspbery pi/oraneg pi.)
Step 2 . Develop application on Linux to display all sampled data and transmit to HDMI port.
Step 3. Convert HDMI signal to 24-bit RGB interface to drive 7" and 10.1" display . datasheets are attached.
I am at step 3 and this is now trouble for me.
I have gone through the TFP401A datasheet but no development boards are available .
Can somebody guide me how to proceed ?
10.1 display SPEC_TST101T-HBD-50A (3).pdf7_displaySPEC_TST070CBOT-01 Serials.pdf