Hi
I need to give 10mV as Op Amp Reference.Input Source voltage is 3.0Volt,i need to develop 10mV .
Advice me a suitable solution
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I need to give 10mV as Op Amp Reference.Input Source voltage is 3.0Volt,i need to develop 10mV .
Advice me a suitable solution
Hi Krishnamoorthy,
Do you have single supply or dual supply? If you have dual supply, you could do something like the following:
The accuracy question is very important as well, the offset voltage is going to directly impact that. The first stage contributes Vos*(1+1/300) and the second stage contributes Vos*(1+1) so the total offset contribution is roughly 3*Vos. In my simulation (attached), a perfect 3V input gives a 10.4mV output, for an error of 4%.
If you only have a single supply, then you'll run into issues with producing such a low output voltage, most rail to rail op-amps can't get that low accurately.
-Paul
Thanks for the quick Reply
My Source voltage 3.0 Volt from CR2032 Battery ( Single Battery only) ,The Input Voltage may decrease up to 2.3 or 2.4.
Advice using Single Supply ,
Thanks and Regards
K.Baskaran
Hi Ronald Michallick
i plan to 10mV is as reference voltage of Amp input ,For the cost reduction Can use signle supply OP AMP or i have to go for dual supply OP Amp ?
Pls see the image
Regards
K
Hi Paul
Cost reduction
Can i go with Single supply OP Amp ( 3+Ve ref to Gnd) OR
I have to go for Dual supply Op Amp ( + 3Volt and - 3Volt)