I see several buffers that are SSTL input and output, to either fan out or buffer an existing SSTL output, but I need a way to convert a standard 3.3V CMOS output to SSTL-2.5
I was hoping I could use a standard voltage level translator, such as SN74AVC16T245 for the job but I'm wondering if there are any better parts. How would you add an SSTL interface to a device that doesn't already have one? (In this case a legacy board with an FPGA that only has 3.3V I/O enabled)
Thanks,
-Andrew