Question about TPS65982(EVM).
When the Source side, 5V/12V/20V supply condition.
⇒customer liked to supply 12V to the Sink side, but it can't be achieved.
Is this a restriction matter of Firmware?
Additional information,
EVM User's guide is 12V to 20V (attached below).
But, Firmware User's guide is 20V (attached below).
Which is correct?
Best regards,
Satoshi