Hello everyone,
I have to drive four 5v loads (located at different position) using single micro-controller pin. My circuit board behaves exactly same we want it to be. However we are bit of confused with voltage level.
P1.0 is micro-controller pin that drives four loads connected with SWOP-1, SWOP-2, SWOP-3, SWOP-4. All four loads are working fine as per P1.0. The doubt we have is with SW. Voltage level measuring at SW is 6.23v when P1.0 is 0v but I think it should be 24v. Is 6.23v okay or it has to be 24v? When we disconnect SW from ULN2803 it measures 24v but when we connect it to IN1 of ULN it becomes 6.23v.
Awaiting response from community members.
Thank you,
Niral