I'm designing a device that has a LiPo battery and a USB connector. USB is used for charging and communication. The on-board microcontroller is powered from either the battery or USB via an integrated 3.3V LDO. 5V is present on board (via a boost converter), but only intermittently.
I am not sure on how to best connect the VCC pin of the TPD2E001. Connecting it to 3.3V makes no sense, 5V isn't always present, so I can either connect it to VBUS or leave open. But connecting it to VBUS of the USB connector means the device won't be protected against surges on VBUS, right?