Dear Sirs,
I am looking for using an A-type connector w/o ID pin for both host and peripheral operation modes.
I need to have the CPU aware of the VBUS direction, as follows:
1. If the external VBUS is active, the CPU shall get the external VBUS and realize that a host is connected, and that it shall operate as peripheral
2. If the ext VBUS is not active, the CPU shall drive it in preparation for a hypothetical slave to be attached.
Can the TPD4S214 operate in such mode?
How shall I connect it in the system?
Thanks,
Avishai