Hi,
About internal pullup resistors of TPD12S016.
The datasheet(SLLSE96F) has the following in "6.5 Electrical Characteristics" ;
RPU(Internal Pulup), SCL_B,SDA_B, Pull-up connected to 5-V rail, "TYP:1.75kohm"
- The MIN&MAX values are not mentioned.
I have considered the reason;
TPD12S016 has "Integrated Pullup and Pulldown Resistors per HDMI Specification"
on the datasheet(page.1). So the MIN/MAX values are mentioned in the HDMI Specification.
(HDMI1.3a specification has the values, min:1.5kohm,max:2.0kohm)
Therefore, the datasheet does not have the MIN&MAX values of internal pullup resistor.
(The MIN&MAX values of internal pullup resistors are the same as the values of HDMI Specification.)
Is this correct?
Thanks in advance.
Best regards,
Takishin