I recently read some articles about some USB devices that are specifically designed to destroy hardware.
"When we connect it up to the USB port, an inverting DC/DC converter runs and charges capacitors to -110V. When the voltage is reached, the DC/DC is switched off. At the same time, the filed transistor opens. It is used to apply the -110V to signal lines of the USB interface. When the voltage on capacitors increases to -7V, the transistor closes and the DC/DC starts. The loop runs till everything possible is broken down."
Do we have any devices or ideas on how someone can design a USB port that could defend against such a device and prevent hardware damage?
Cheers,
Joe Howard