Dear all,
I need to make an I2C level translation beetween a 1.8V master and a 3V slave. For BOM optimization, I'm considering the PCA9306 (I'm using it for 1.2 to 3.3V I2C translation on the same board). I understand that the 1.8V supply should be on VREF1, the 3V on (VREF2+EN) through a ~200kOhm for proper component biasing.
The question is : My 3V will always be on, whereas sometimes (eco mode) the 1.8V will be shutdown. Does the PCA9306 isolates the 2 interfaces in this case or is there any currents flowing from SDA2 to SDA1, SCL2 to SCL1, VREF2 to VREF1?
I've also read on this forum some unanswered questions about the proper resistor biasing of the device, some having to increase the 'VREF2+EN' resistor value. What is the acceptable range for this value? Does it depends of RPU?
With best regards,
Thibault